Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is the resonator clock input used as count clock of the watchdog timer?

Latest Updated:04/01/2006

Question:

Is the resonator clock input used as the count clock of the watchdog timer?

Answer:

No, it is not.
For details about the watchdog timer operation, refer to the user's manual of each device.

[Explanation]
Usually, a divided main system clock (fx) is used as the watchdog timer's count clock.
For example, fx/256 is used in the uPD780034A Subseries and fx/128 or the subsystem clock is used in the uPD784216A Subseries.
In the 78K0/Kx1, either the X1 oscillation clock divided by 16 or the internal oscillator divided by 4 is used as the watchdog timer's count clock.

Suitable Products
78K Family