Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Reference Materials for Migration from H8 to RL78

Last Updated:05/10/2018

Question:

I'm currently using the H8. Do you have any reference material regarding migration to the RL78?

Answer:

We have the following reference materials available.

・Guide for migration from H8/3687 to RL78/G14 for each peripheral function

  Guide for migrating from H8/3687 to RL78/G14 for each peripheral function

  I/O PortsNote

  Interrupts (Exception Handling)Note

  Clock GeneratorNote

  Timer RDNote

  Note:There is no sample code in the target application note.

・Development environment
  Please click here for the Guide for migrating the development environment.

Suitable Products
RL78/G10
RL78/G11
RL78/G12
RL78/G13
RL78/G14
RL78/G1A
RL78/G1C
RL78/G1D
RL78/G1E
RL78/G1F
RL78/G1G
RL78/G1H
RL78/I1A
RL78/I1C
RL78/I1D
RL78/I1E
RL78/L12
RL78/L13
RL78/L1A
RL78/L1C