Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Reference Materials for Migration from M16C to RL78

Last Updated:05/10/2018

Question:

I'm currently using the M16C. Do you have any reference material regarding migration to the RL78?

Answer:

We have the following reference materials available. 

・Software for converting a C source file for NC30 to a C source file for CC-RL
  CcnvNC30 C Source Code Converter

・Guide for migration from M16C/62P to RL78/G14 for each peripheral function

  Guide for migrating from M16C/62P to RL78/G14 for each peripheral function

  I/O PortsNote

  InterruptsNote

  A/D ConverterNote

  Clock GeneratorNote

  Note:There is no sample code in the target application note.


・Comparison of peripheral functions
  M16C/65C Group and RL78/G13, RL78/G14 Peripheral Function Comparison between M16C/65C Group and RL78/G13, RL78/G14
 
・[Reference] How to replace a program for R8C with a program for RL78
  Replacement Guide for R8C Family to RL78 Family (CcnvNC30) 

・Development environment
  Please click here for the Guide for migrating the development environment.

Suitable Products
RL78/G10
RL78/G11
RL78/G12
RL78/G13
RL78/G14
RL78/G1A
RL78/G1C
RL78/G1D
RL78/G1E
RL78/G1F
RL78/G1G
RL78/G1H
RL78/I1A
RL78/I1C
RL78/I1D
RL78/I1E
RL78/L12
RL78/L13
RL78/L1A
RL78/L1C