Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What are cares at N-ch open-drain output mode ?

Latest Updated:07/26/2016

Question:

What are cares at N-ch open-drain output mode ?

Answer:

Shoot- through-current on input buffer may occur according to voltage of terminal pins even if it is N-ch open-drain output mode, because input buffer is on-state in output mode.
 
Suitable Products
RL78/F12
RL78/F13
RL78/F14
RL78/F15
RL78/D1A