Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Why does oscillation of main clock stops even if it's not on STOP mode?

Latest Updated:04/01/2006

Question:

Oscillation of the main clock stops even though I have not executed a STOP instruction.
I do not think there is a problem with the program as it has already been checked using an emulator.

Answer:

Is there oscillator matching?
Normal oscillation cannot be obtained unless there is oscillator matching.
Suitable Products
RL78 Family
78K Family