Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

uPD784218: SIO2 and UART: Pin 39 (ASCK2) as I/O port?

Latest Updated:12/01/2011

Question:

In the uPD784218, during use of SIO2 with the internal clock and use as UART, can I use pin 39 (ASCK2) as an I/O port?

Answer:

Yes.
When using the internal clock for the serial clock, ASCK2 (pin 39) can be used as a port.
Suitable Products
RL78 Family
78K Family