Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Does the output from the TMO pin set to low level?

Latest Updated:06/10/2013

Question:

When the CKS bit and CSS bit of the TMR.TCCR register are cleared to 0, the TMR counter stops. Is the output from the TMO pin also set to low level?

Answer:

TMO does not necessarily go to low level when the CKS bit and CSS bit of the TMR.TCCR register are cleared to 0. The value (level) at the time the counter stopped is retained.
Suitable Products
RX62N, RX621
RX610
RX630
RX63N, RX631
RX210
RX220