Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

External clock: is it necessary to connect resistance in EXTAL & XTAL?

Latest Updated:06/20/2013

Question:

When inputting an external clock, is it necessary to connect resistance between EXTAL and XTAL?

Answer:

It is not necessary.
Suitable Products
RX62N, RX621
RX62T
RX610
RX62G
RX630
RX63N, RX631
RX63T
RX210
RX220
RX110
RX111
  • Was this article helpful?