Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Features of the CPU core of the new RX65N/RX651 MCUs

Last Updated:11/13/2017

Question:

What are the features of the CPU core of the new RX65N/RX651 MCUs?

Answer:

The new MCUs are based on the high-performance RXv2 core and a 40nm process, which provide strong power efficiency for CPU operation at 4.55 Core Mark/MHz.
Suitable Products
RX65N, RX651