Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How many overhead there is aside from handling routine written by user?

Latest Updated:06/20/2013

Question:

In the outline of the exception handling procedure shown in the user's manual: hardware, how many clocks are required for hardware pre-processing, post-processing, and branching to vector read handling? I'd like to know how much overhead there is in addition to the exception handling routine written by the user.

Answer:

See Numbers of Cycles for Response to Interrupts in the CPU chapter of the user's manual: hardware.
Suitable Products
RX62N, RX621
RX62T
RX610
RX630
RX63N, RX631
RX210
RX220
RX110
RX111