Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to use all pins in program debugging while using it for user signals?

Latest Updated:05/27/2013

Question:

I need to use all the pins of an RX microcontroller. Is there any way to carry out program debugging while also using debug pins for user signals?

Answer:

Renesas offers a debug MCU board for low pin count devices. If this board is used, debug pins can also be used for user signals.
Suitable Products
RX62N, RX621
RX62T
  • Was this article helpful?