Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to write a user boot program to the user boot area (user boot mat)?

Latest Updated:06/20/2013

Question:

I want to write a user boot program to the user boot area (user boot mat). How should I do this?

Answer:

The user boot area can only be programmed/erased in boot mode.
Start in boot mode and write to the user boot area (user boot mat).
Suitable Products
RX62N, RX621
RX62T
RX610
RX62G
RX630
RX63N, RX631
RX63T
RX210
RX220
  • Was this article helpful?