Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

MCU Functionality Problems at Higher Frequencies

Last Updated:06/08/2017

Question:

My MCU does not work properly with higher operational frequencies.  What are the possible causes?

Answer:

Please check the following items:

1) Make sure that both the operating frequency and operating voltage are set within the allowable range.

2) Depending on the MCU, you must change the access cycles of the operational power control state, code flash, RAM, etc.  To change the access cycles, check the operational power control register (OPCCR), or the MEMWAIT bit setting of the memory cycle wait setting register (MEMWAIT).

Suitable Products
RX110
RX111
RX113
RX210
RX21A
RX220
RX62N, RX621
RX62T
RX62G
RX630
RX63N, RX631
RX63T
RX64M
RX71M
  • Was this article helpful?