Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What is the meaning of the -DS at the end of a IRQ pin?

Latest Updated:08/10/2012

Question:

What is the meaning of the -DS at the end of a IRQ pin?

Answer:

Pin names suffixed with -DS can be used to cancel deep software standby mode.

Suitable Products
RX630
RX63N, RX631
RX210