Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Cortex-R4 Processor with FPU Reference Documents

Last Updated:09/27/2017

Question:

Where can I get documents about ARM Limited as it relates to the Cortex-R4 Processor with FPU?

Answer:

You can get pertinent documents from the following sites:

○ Cortex-R4F Technical Reference Manual
   http://infocenter.arm.com/help/topic/com.arm.doc.ddi0363g/index.html

○ ARM Architecture Reference Manual ARMv7-A and ARMv7-R edition Issue C 
   http://infocenter.arm.com/help/index.jsp?topic=/com.arm.doc.ddi0406c/index.html

Note : If the exact address of the site has changed, the link may not function.
            If this is the case, please search for the keyword of the document.

Suitable Products
RZ/T1
  • Was this article helpful?