Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is the JPEG codec (hard IP) built in?

Latest Updated:12/02/2015

Question:

Is the JPEG codec (hard IP) built in?

Answer:

The JPEG codec (hard IP) is not built in.
Suitable Products
RZ/G1E
RZ/G1M
  • Was this article helpful?