Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

RSTOUT Pin to Reset Boot Flash Memory Module

Last Updated:09/27/2017

Question:

Is it possible to use RSTOUT# as a reset signal for the Flash Memory Module used to boot?

Answer:

The RSTOUT# signal cannot be used with the Flash Memory for boot.  It is recommended to use the RES# signal and others.

RSTOUT# can be used as a reset signal to other external devices, if the RSTOUT# pin outputs low level for 500 us (typ.) when reset occurs with RES# signal.  As boot processing of the RZ/T1 starts after reset releases the RES# pin, there is a possibility that reading from the flash memory may not be ready in time when RSTOUT# pin is used as reset for flash memory.

For more details, refer to RZ/T1 Group User’s Manual: Hardware (R01UH0483) "6.3.6 Reset Output Pin (RSTOUT#)".

Suitable Products
RZ/T1