Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What are the packages for RZ/G?

Latest Updated:05/06/2016

Question:

What are the packages for RZ/G?

Answer:

Packages are as follows.
RZ/G1E: Flip Chip BGA, 501-pin, 21 x 21 mm, 0.8 mm ball pitch
RZ/G1N, RZ/G1M: Flip Chip BGA, 831-pin, 27 x 27 mm, 0.8 mm ball pitch
Suitable Products
RZ/G