Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What is the average efficiency for the theoretical value of the DDR memory bus band?

Latest Updated:12/02/2015

Question:

What is the average efficiency for the theoretical value of the DDR memory bus band?

Answer:

The average efficiency of 32-bit connected DDR memory is in general about 60%.
Suitable Products
RZ/G1E
RZ/G1M