Can CPU processing keep running when DMAC/DTC is using internal bus?
Latest Updated:03/21/2012
Question:
Can the CPU processing keep running when the DMAC or DTC is using the internal bus?
Answer:
If the processing requires only one bus: CPU bus, F bus, or M bus, the processing can keep running when the DMAC or DTC is using the internal bus.
Suitable Products
SH7285, SH7286 |
SH7243 |
SH7214, SH7216 |
SH7231 |
SH7239, SH7237 |
SH7211 |