Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Can data MAT in data flash be kept when rewriting on-chip flash memory?

Latest Updated:09/11/2012

Question:

Can the content of the data MAT in the data flash (FLD) be kept when rewriting the on-chip flash memory (User MAT) in the user program mode?

Answer:

The data in the data flash (FLD) will be kept during execution of the user program mode.
Suitable Products
SH7214, SH7216
SH7231
SH7239, SH7237