Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Does pass-through current flow when the midpoint of VCC and GND is in?

Latest Updated:03/23/2009

Question:

In the general input pins sharing with an analog input, does a pass-through current flow when the midpoint potential of VCC and GND is entered?

Answer:

When it is used as an analog input, a pass-through current must not flow even if an input voltage is midpoint potential.

However, when it is used as a general input and an input voltage is midpoint potential, a pass-through current flows. In addition, you should be aware that the characteristic of LSI is deteriorated and it may cause a fatal distruction when the pass-trough current flows over a long duration.

Suitable Products
SH7144, SH7145
SH7065
SH7047, SH7049, SH7105, SH7107, SH7109
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7032
SH7018
SH7014, SH7016, SH7017