Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Does the CS signal turn to H after accessing the SC space on on-chip RAM ?

Latest Updated:09/11/2012

Question:

In the SH family, when accessing to the on-chip RAM after accessing to the SC space, does the CS signal turn to "H" level (get negated)?

Answer:

The CS signal shall be asserted only when accessing to the external space of the address and shall be negated to "H" level in the other areas.
Suitable Products
SH7285, SH7286
SH7243
SH7214, SH7216
SH7231
SH7239, SH7237
SH7211
SH7146, SH7149
SH7131, SH7132, SH7136, SH7137
SH7083, SH7084, SH7085, SH7086