FPU instruction supported by SH-2E is also supported by SH-2A?
Latest Updated:03/23/2009
Question:
FPU instruction supported by SH-2E is also supported by SH-2A?
Answer:
SH-2A has the lineup in two kinds of CPU cores such as "SH-2A" and "SH2A-FPU".
"SH-2A" doesn't have the instruction related to FPU of "SH-2E" though "SH2A-FPU" supports "SH-2E" instruction.
Meanwhile, SH7206 is a product with on-chip CPU core of "SH-2A".
Suitable Products
SH7206 |