Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to transmit the SCI 10-byte data using the DTC function?

Latest Updated:09/11/2012

Question:

I'm trying to transmit the SCI 10-byte data using the DTC function. The DTC transfers 10-byte data to the TDR of the SCI,  but only 9-byte data is tranmitted from the SCI.

Answer:

The SCI transmitter/receiver uses double-buffering.
When the TXI interrupt occurs after the 10-byte data transfer has been completed by the DTC, 10th byte of the data has not been transmitted yet from the the SCI.  Follow the procedure as follows to clear the TE;
Clear the TEND flag during the TXI interrupt generated after the 10-byte data transfer has been completed by the DTC, and allow the TEI interrupt. Clear the TE during the TEI interrupt generated after the data transmission of 10th byte has been completed.

Also, clear the TDRE flag during the TXI interrupt generatedafter the 10th byte transfer has been comopleted by the DTC (activation source flag cannot be cleared by the last transfer of theDTC).
The last data in the transmit data register (SCTDR) written by the DTC cannot be transferred to the transmit shift register (TSR) if the TDRE is not cleared.

Suitable Products
SH7285, SH7286
SH7214, SH7216
SH7231
SH7239, SH7237
SH7211
SH7147
SH7146, SH7149
SH7131, SH7132, SH7136, SH7137
SH7083, SH7084, SH7085, SH7086