Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is it possible to execute program on external memory and erase on chip?

Latest Updated:03/25/2009

Question:

Is it possible to execute a program on the external memory and erase/rewrite to the on-chip flash memory in the user programming mode?

Answer:

Yes, it is possible.
However, it is necessary to control the wait time, when erasing or rewriting to the on-chip flash memory. Please note that the access time of the external memory needs to be considered, if the wait time is controlled by a software timer.
Suitable Products
SH7144, SH7145
SH7065
SH7058
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7018
SH7014, SH7016, SH7017