Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is the interrupt of vector number reserved by system likely generated?

Latest Updated:03/25/2009

Question:

Is there a possibility that the interrupt of the vector number reserved by system gets generated in the Exception Processing Vector Table?

Answer:

No, the interrupt of the vector number reserved by system never gets generated because the Interrupt Controller does not fetch the vector reserved by system.
Also, the vector reserved by system cannot be used.
Suitable Products
SH7144 Series
SH7060 Series
SH7050 Series
SH7047 Series
SH7046 Series
SH7040 Series
SH7030 Series
SH7020 Series
SH7010 Series