Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Is the operation in the True IDE mode possible?

Latest Updated:03/23/2009

Question:

In the PCMCIA interface of SH7709S/SH7729R/SH7706, is the operation in the True IDE mode possible?

Answer:

The PCMCIA interface of SH7709S/SH7729R/SH7706 is "IC memory card and I/O card interface" provided by the JEIDA specification Ver4.2 (PCMCIA2.1).

It doesn't support the True IDE mode.

Suitable Products
SH7729R
SH7709S
SH7706