Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What are temperature ranges during usage of SuperH Family product?

Latest Updated:03/25/2009

Question:

Is the temperature range during usage of SuperH Family indicated in each type number?
In addition, what are the temperature ranges during usage of each SuperH Family product?

Answer:

The type number indication and temperature range during usage of each product are shown in the following table.
The quality and temperature range during usage of each product are indicated by a suffix attached to a product name such as "W", "D" or "J".

Example)
Case of SH7047F:
HD64F7047F40: Standard product/temperature range during usage -20~75C
D64F7047FW40: Standard product/temperature range during usage -40~85C
HD64F7047FJ40: High-quality product/temperature range during usage -40~85C

The temperature ranges during usage of each SuperH Family product are listed in the following table.

image

Suitable Products
SH7144, SH7145
SH7058
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054
SH7047, SH7049, SH7105, SH7107, SH7109
SH7046, SH7148, SH7101, SH7048, SH7104, SH7106, SH7108
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7018
SH7014, SH7016, SH7017
SH7011