Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What data should be written to flame memory (display dot location)?

Latest Updated:03/24/2009

Question:

When I want to display palette colors which set to LCDC palette data registers (LDPR00 to FF), what data should be written to flame memory (display dot location)?

Answer:

When using the palette, 8-bit data in flame memory specifies the palette number. The LCDC takes color and gradation data from the specified palette numbers and send it to liquid crystal module.
Suitable Products
SH7727
SH7720