Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What the setting to change to the DSP arithmetic mode?

Latest Updated:03/25/2009

Question:

What the setting to change to the DSP arithmetic mode?

Answer:

The DSP arithmetic mode is set by bit 12(DSP bit) of status register (SR).

When DSP bit = "1" is set, the DSP instruction becomes effective.

Suitable Products
SH7729R
SH7727
SH7720
SH7710
  • Was this article helpful?