Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What transfer request is the set value of DMAC DMATCR?

Latest Updated:03/23/2009

Question:

Is the set value of DMAC DMATCR the number of transfers for one transfer request or the number of transfer request accepts?

Answer:

Answer
Suitable Products
SH7065
SH7058
SH7055