Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

What value to set to CKS of the SCSMR and to SCBRR when using SCI?

Latest Updated:03/21/2012

Question:

When using SCI in asynchronous mode with an external clock input, what value should I set to CKS of the SCSMR, and to SCBRR?

Answer:

No specific setting is required for CKS of the SCSMR and SCBRR when using them with external clock input.
Suitable Products
SH7285, SH7286
SH7243
SH7214, SH7216
SH7239, SH7237
SH7211
SH7124, SH7125
SH7146, SH7149
SH7083, SH7084, SH7085, SH7086