Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Which specs of tOE or tACC has a priority?

Latest Updated:03/25/2009

Question:

As for SuperH microcomputer bus timing, spec of tRDS(read data set up time) is specified. Which specs of tOE(access time from read strobe) or tACC(read data access time) has a priority? 

Answer:

The rules of tRDS are the specification that is assumed the connection with an external device working by clock synchronization.

Please follow the rules of tRDS when connecting with an external device working by clock synchronization.

On the other hand, the rules of tOE and tACC are the specification that is assumed the connection with an external device working by clock asynchronization.

Please follow the rules of tOE and tACC when connecting with an external device working by clock asynchronization.

Suitable Products
SH7144, SH7145
SH7065
SH7058
SH7055
SH7050, SH7051
SH7052, SH7053, SH7054
SH7047, SH7049, SH7105, SH7107, SH7109
SH7040, SH7041, SH7042, SH7043, SH7044, SH7045
SH7032, SH7034, SH7034B
SH7032
SH7020, SH7021
SH7018
SH7014, SH7016, SH7017
SH7011