Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

How to make an external interrupt occur with ID bit of PSW set to 0?

Latest Updated:12/01/2011

Question:

I want an external interrupt to occur but the interrupt request is not acknowledged.
The ID bit of the PSW is set to 0, the interrupt request is reset, and interrupt processing is enabled.

Answer:

Possible causes are as follows: - A mask is set for the interrupt (bit 6 of the interrupt control register is set).
- NMI processing is in progress (the NP bit of the PSW is set).
- Processing of a higher priority interrupt is in progress (check using the ISPR register.)
- Consecutive instructions that do not acknowledge an interrupt exist.

Check the PSW, ISPR, and the interrupt control register.

Suitable Products
V850 Family