Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Can we carefully regard to board layout of USB host controller?

Latest Updated:06/01/2006

Question:

Is there any to be careful of in regards to board layout of the USB host controller?

Answer:

Please refer to USB 2.0 PCB Design Guide.
Analog circuit and USB differential signals should be routed carefully to prevent noise.
Suitable Products
CMOS Operational Amplifiers
Bipolar Operational Amplifiers