Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

Does BUSY output become low after data n and rising edge of the STB input?

Latest Updated:08/01/2005

Question:

When the operation is executed as described in "Application" of the uPD16430A Data Sheet, does BUSY output become low after the writing data n and rising edge of the STB input?

Answer:

Yes, it does.
Suitable Products
CMOS Operational Amplifiers
Bipolar Operational Amplifiers