Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

TPS-1 Response to a Watchdog Error

Last Updated:06/01/2017

Question:

When a watchdog error occurs, will the TPS-1 first set the output WD_OUT then self reset automatically?

Answer:

An internal watchdog error forces TPS-1 into reset and the subsequent boot process. This process includes setting WD_OUT high, thus clearing the WD_OUT alarm to the host CPU.
Suitable Products
TPS-1
  • Was this article helpful?