Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

USB hub controller: Possibility of ROM shared with other devices?

Latest Updated:06/01/2006

Question:

For the USB hub controller, can serial ROM for hub controller be shared with other devices?

Answer:

No, it is not possible. A serial ROM is used solely by the hub controller.
Suitable Products
CMOS Operational Amplifiers
Bipolar Operational Amplifiers