Skip to main content
Knowledgebase
Home
Renesas India - Knowledgebase

TPS-1 Functional Safety IEC61508

Last Updated:06/01/2017

Question:

Can the TPS-1 meet the functional safety standard IEC61508?

Answer:

The IEC61508 standard belongs to electrical or electronic systems. The TPS-1 can be seen as part of a system, but the TPS-1 itself will not be certified as a safety element. The TPS-1 is a communication controller, whereas the safety issue will be implemented in the application protocol, meaning the main communication layer. For this purpose you can use the PROFIsafe application (safe communication layer).
Suitable Products
TPS-1